Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22496
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/21 17:15
  • Print

Number of modules that can be synchronized using the MELSEC iQ-R series inter-module synchronization function

How may modules can be synchronized using the MELSEC iQ-R series inter-module synchronization function?
Category : 

Answer

The number of modules that can be synchronized is as follows.
- In single CPU system configuration: 64 modules
- In multiple CPU system configuration: 57 to 63 modules

Mounting positions of the modules and the maximum number of mountable modules do not change regardless of whether
the inter-module synchronization function is used or not.

Since RnENCPU occupies two slots, one or more slots are occupied, so the maximum number of installable modules decreases.
Product Name
MELSEC iQ-R Series
Series
MELSEC iQ-R Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries