Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22533
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/20 14:43
  • Print

Error code "4100" in QCPU

The error code "4100" is displayed on QCPU.
The instruction in which the error occurs is [D/ D6270 D6268 D6268]. Are there any remedies?
Category : 

Answer

The error code "4100" is "OPERATION ERROR".
The error occurs when a number is divided by 0 (Divisor D6268 value is 0).
Make modifications so that the divisor is other than 0 when it is executed.
Product Name
MELSEC-Q Series
Series
Q (Q mode)

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries