Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22566
  • Release Date : 2018/09/03 17:29
  • Print

Recommended cables for MODBUS(R) interface module QJ71MB91

Which types of cables should be used for QJ71MB91?
Category : 

Answer

The RS-232 cable should meet RS-232 standards and not exceed 15 m in length.
The RS-422/485 cable should meet specifications described in the following manual not exceed 1200 m in length.
- "MODBUS (R) Interface Module User's Manual" Section 3.3.2
Product Name
MELSEC-Q Series
Series
MODBUS

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries