Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22571
  • Release Date : 2018/09/03 17:29
  • Print

How to turn OFF the "COM.ERR" LED of the Ethernet module

Is it possible to turn OFF the "COM.ERR" LED of an Ethernet module installed to the standby system of a redundant system?
Category : 

Answer

The LED can be turned OFF by operations from GX Developer. The operation method is as follows.

(1) Connect to the CPU in the standby system in Transfer Setup.
- Connect to the CPU in the standby system with "No specified system" selected.

(2) Turn off the "COM.ERR" LED.
- Click the "COM.ERR off" button in Ethernet diagnostics dialog box.
Product Name
MELSEC-Q Series
Series
CPU

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries