Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22573
  • Release Date : 2018/09/03 17:29
  • Print

Auto refresh setting in GX Configurator -MB

What is auto refresh setting in GX Configurator -MB for MODBUS (R) interface module?
Category : 

Answer

Auto refresh setting is for storing the buffer memory data of a MODBUS (R) interface module to specified devices of a CPU module and for storing device data of the CPU module to the buffer memory automatically.
Auto refresh setting is required when the master function is used, but not required when only the slave function is used.
Product Name
MELSEC-Q Series
Series
MODBUS

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries