FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Boot operation from the standard ROM in the universal model QCPU
FAQ
Boot operation from the standard ROM in the universal model QCPU
Does the universal model QCPU module have standard ROMs, and is it possible to boot from it?
- Category :
Answer
The universal model QCPU modules have their standard ROM but boot operation from the standard ROM is impossible.
Boot the module from a memory card.
Boot the module from a memory card.
- Product Name
- MELSEC-Q Series
- Series
- CPU
May I have your opinion?
Related FAQ
- Setting of Q series registers whose data is held when a power failure occurs
- Reading and writing bits/words using the FL-net (OPCN-2) interface module
- Returning to the overwrite mode in GX Developer
- Label programs in GX Works2
- What to do in the case of the error "A default router IP address needs to be set."