FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Creating comments both in English and in Japanese
FAQ
Creating comments both in English and in Japanese
Is it possible to create two comments, one in English and the other in Japanese, and switch them for display in GX Works2?
- Category :
Answer
Create global device comments and local device comments in respective languages.
The device comments can be switched in [Options] -> [Tool].
The device comments can be switched in [Options] -> [Tool].
- Product Name
- Engineering Software
- Series
- Software Package (GPP function)
May I have your opinion?
Related FAQ
- How to read the device memory in GX Works2
- MODBUS(R) interface module's involvement in master and slave stations
- Settings of the built-in Ethernet port of the universal model QCPU
- COMMENT to disappear after a PLC type change
- Reading file registers simultaneously with the program, parameters, and other data in GX Works2