Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22651
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/26 16:53
  • Print

Clock function accuracy

What does the following information on the basic model QCPU's clock function denote?
 - Accuracy: -2.57 to +5.27s(TYP.+2.22s)/d at 25 degrees Celsius.
Category : 

Answer

It means that in an ambient temperature of 25 degrees Celsius, an error per day falls within the range of "delay of 2.57s" to "advance of 5.27s".
"TYP.+2.22s" denotes that the standard value is "advance of 5.27s".
Product Name
MELSEC-Q Series
Series
CPU

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries