Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22654
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/21 12:02
  • Print

QCPU built-in Ethernet port setting when using the simple PLC communication function

What settings are necessary for the built-in Ethernet port QCPU on the external device side when using the simple PLC communication function?
Category : 

Answer

The following settings are required for the "Open Setting" for the number of connected external devices.
 - Protocol: "UDP"
 - Open System: "MELSOFT connection"
Product Name
MELSEC-Q Series
Series
Q (Q mode)

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries