Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22729
  • Release Date : 2018/09/03 17:29
  • Print

Error code "2400" in LCPU

The error code "2400" is displayed on LCPU.

The individual information parameter number is "7000". Are there any remedies?
Category : 

Answer

The error code "2400" is "FILE SET ERROR".
This error may be caused when the file specified with a parameter does not exist.
The individual information parameter number "7000H" corresponds to program settings.
Check whether the program set in the program setting is identical to the program stored in the CPU.
Product Name
MELSEC-L Series
Series
CPU

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries