FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Use of an A-compatible 1E frame for the built-in Ethernet port of LCPU
FAQ
Use of an A-compatible 1E frame for the built-in Ethernet port of LCPU
Can I use an A-compatible 1E frame of the MC protocol for the built-in Ethernet port in the L series CPU?
- Category :
Answer
The built-in Ethernet port in the L series is compatible only with a QnA-compatible 3E frame of the MC protocol. An A-compatible 1E frame is not supported.
- Product Name
- MELSEC-L Series
- Series
- L Series
May I have your opinion?
Related FAQ
- MC protocol compatibility of the built-in Ethernet port
- Simultaneous use of simple PLC communication function and socket communication
- Loop disconnection detection function and heater disconnection detection function of temperature control module
- Sample comments for special relays/registers
- Battery replacement for LCPU