Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22739
  • Release Date : 2018/09/03 17:29
  • Print

LCPU built-in Ethernet port setting when using the simple PLC communication function

What settings are necessary for the L series CPU on the external device side when using the simple PLC communication function?
Category : 

Answer

The following settings are required for the "Open Setting" for the number of connected external devices.
- Protocol: "UDP"
- Open System: "MELSOFT connection"
Product Name
MELSEC-L Series
Series
L Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?