Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22751
  • Release Date : 2018/09/03 17:29
  • Print

SD1282 of LCPU with built-in Ethernet port

During socket communication of L series CPU with built-in Ethernet port, how does the special register SD1282 (Open completion signal) correspond to the connection number?
Category : 

Answer

The bits 0 to F of the special register SD1282 (Open completion signal) correspond to the connection numbers 1 to 16. When the open processing is completed, the corresponding bit will turn ON.
Product Name
MELSEC-L Series
Series
L Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries