FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Versions of LCPU compatible with LJ71E71-100
FAQ
Versions of LCPU compatible with LJ71E71-100
From what version does the L series CPU support LJ71E71-100?
- Category :
Answer
The L series CPU serial numbers with upper 5 digits of "14112" or later indicate compatibility with LJ71E71-100.
- Product Name
- MELSEC-L Series
- Series
- L Series
May I have your opinion?
Related FAQ
- Versions of built-in Ethernet port LCPU compatible with SNTP function
- PLC write not possible due to memory overload
- Execution of the SOCRMODE instruction in the same connection during socket communication of LCPU
- Simultaneous broadcast reception setting for built-in Ethernet port LCPU
- Maximum number of connectable modules to LCPU when it is not extended