FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Execution of the SOCRMODE instruction in the same connection during socket communication of LCPU
FAQ
Execution of the SOCRMODE instruction in the same connection during socket communication of LCPU
I would like to change the receive data size by each reception during socket communication of L series CPU. Is it possible to repeat the SOCRMODE instruction to the same connection?
- Category :
Answer
It can be executed for the same connection number. When data exist in the socket communication receive data area and the SOCRMODE instruction is executed, values take effect after the SOCRCV/SOCRCVS instruction is executed once.
- Product Name
- MELSEC-L Series
- Series
- L Series
May I have your opinion?
Related FAQ
- Simultaneous broadcast reception setting for built-in Ethernet port LCPU
- Maximum number of connectable modules to LCPU when it is not extended
- How to use PWM output of LCPU built-in I/O
- Versions of built-in Ethernet port LCPU compatible with SNTP function
- Remedy to an error message when performing online change in LCPU