FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > L60DA4 accuracy
FAQ
L60DA4 accuracy
What is the accuracy of L60DA4?
- Category :
Answer
- Ambient temperature: 25+/-5 degrees Celsius with tolerance of +/-0.1%
- Ambient temperature: 0 to 55 degrees Celsius with tolerance of +/-0.3%
(accuracy for the maximum analog output value)
- Ambient temperature: 0 to 55 degrees Celsius with tolerance of +/-0.3%
(accuracy for the maximum analog output value)
- Product Name
- MELSEC-L Series
- Series
- D / A Conversion Unit