Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22827
  • Release Date : 2018/09/03 17:30
  • Update : 2018/09/22 15:24
  • Print

Resolution provided for L60AD4

Does the resolution provided for L60AD4 become higher if the analog input range is set to "User range setting" and the analog input value corresponding to the maximum digital output value is set to a smaller value using the gain setting?
Category : 

Answer

The maximum resolution for the user range setting does not change.

Product Name
MELSEC-L Series
Series
A / D Conversion Module

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries