Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22840
  • Release Date : 2018/09/03 17:30
  • Update : 2018/09/22 13:22
  • Print

File export of ladder programs

Is it possible to export/import a ladder program created using GX Developer to/from a text file or an Excel-format file in list (mnemonic) representation? Can the operation above also be performed for device comments?
Category : 

Answer

(1) If only GX Developer is used
     - The operation cannot be carried out for ladder programs. 
     - For device comments, copy and paste operations can be carried out with GX Developer and Excel simultaneously opened.
       Match the column and row designations of Excel with GX Developer.

(2) If GX Developer and GX Converter (SW[ ]D5C-CNVW) are used
      Ladder programs and device comments of GX Developer can be converted into text-format or CSV-format data. Also,
      programs and device comments created in text-format or CSV format can be imported into GX Developer.
Product Name
Engineering Software
Series
Software Package (GPP function)

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries