Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22967
  • Release Date : 2018/09/03 17:31
  • Update : 2018/09/25 13:20
  • Print

Precautions taken when QJ61BT11 is replaced with QJ61BT11N

Are there any precautions that must be followed when QJ61BT11 is replaced with QJ61BT11N?
Category : 

Answer

Set the Network Parameter as shown below.
(1) If QJ61BT11 is in the remote net mode, use the remote net Ver.1 mode for QJ61BT11N.
(2) If QJ61BT11 is in the remote I/O net mode, use the remote I/O net mode for QJ61BT11N.

For more details, refer to the following manual.
 - CC-Link System Master/Local Module User's Manual
   Appendix 5 Difference from traditional modules
   Appendix 5.2 Precautions when replacing a QJ61BT11 with a QJ61BT11N
Product Name
Network Related Products
Series
CC-Link

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries