FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Difference in specifications between CC-Link versions
FAQ
Difference in specifications between CC-Link versions
What are the differences between CC-Link Version 1.00, 1.10, and 2.00?
- Category :
Answer
Ver.1.10 is a standard where CC-Link station-to-station cable length restriction in Ver. 1.00 has been removed, and the length of all station-to-station cables is 20 cm or longer. Ver.1.00 is a traditional standard. Ver.2.00-compatible module is a module that supports the cyclic point expansion. The specifications of a cable are the same as those of Ver.1.10.
- Product Name
- Network Related Products
- Series
- CC-Link
May I have your opinion?
Related FAQ
- QJ71E71-100's compatibility with the automatic cable type (straight or cross) recognizing function
- Intelligent Buffer Select of the CC-Link parameter
- Difference in specifications between "AJ65BT" and "AJ65SBT" in CC-Link remote I/O modules' model names
- How to set the numbers of occupied stations for CC-Link local stations
- Difference between AJ65SBTB1-16DT1 and AJ65SBTB1-16DT2