Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22992
  • Release Date : 2018/09/03 17:31
  • Print

Buffer memory addresses of CC-Link modules

I want to write and read data using FROM/TO instructions in CC-Link communication. Does each station number have fixed buffer memory addresses for them to be assigned?
Category : 

Answer

If the remote net Ver.1 mode is used, each station number is given fixed buffer memory addresses.
If the remote net Ver.2 mode is used, different buffer memory addresses are given according to the type of slave station and the number of points the slave station takes.
Product Name
Network Related Products
Series
CC-Link

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries