FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Communication between a CC-Link master station and local stations
FAQ
Communication between a CC-Link master station and local stations
How do I establish the CC-Link communication between a master station and local stations?
- Category :
Answer
There are two modes of transient transmission, cyclic transmission and transient transmission, for the communication between a master station and a local station.
(1) Cyclic transmission
Bit information (remote input RX and remote output RY) and word information (remote register RWw, RWr)
allows N: N data communications between programmable controller CPU modules.
(2) Transient transmission
Data in the buffer memory of a local station and CPU module's devices can be read and written with desired timing.
(1) Cyclic transmission
Bit information (remote input RX and remote output RY) and word information (remote register RWw, RWr)
allows N: N data communications between programmable controller CPU modules.
(2) Transient transmission
Data in the buffer memory of a local station and CPU module's devices can be read and written with desired timing.
- Product Name
- Network Related Products
- Series
- CC-Link