FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Read and write operations for CC-Link buffer memory
FAQ
Read and write operations for CC-Link buffer memory
Are there any problems if data is written into and read from the buffer memory using a FROM/TO instruction without the refresh device setting of the CC-Link parameter?
- Category :
Answer
There is no problem in writing/reading data into/from the buffer memory using a FROM/TO instruction with the refresh device setting left blank.
The refresh device setting and a FROM/TO instruction cannot be used concurrently.
The refresh device setting and a FROM/TO instruction cannot be used concurrently.
- Product Name
- Network Related Products
- Series
- CC-Link