FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Connecting terminating resistors for CC-Link communication
FAQ
Connecting terminating resistors for CC-Link communication
Do I have to connect a terminating resistor to a CC-Link master station?
- Category :
Answer
Connect terminating resistors to both ends of physical cables.
A master station is not necessarily required to be connected to either end of its network.
A master station is not necessarily required to be connected to either end of its network.
- Product Name
- Network Related Products
- Series
- CC-Link
May I have your opinion?
Related FAQ
- Connecting AJ65BT-R2N to a GOT
- RS-485 connection between LJ71C24 and an external device
- Continuous executions of protocols by the QJ71C24N series CPRTCL instruction
- Applicable size for plug-in connector socket block on QJ71C24N-R4
- Order in which a CC-Link master module and slave stations are connected