Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23052
  • Release Date : 2018/09/03 17:31
  • Print

32-bit data assurance

What is the setting required to prevent 32-bit data from being separated in the CC-Link IE Controller Network?
Category : 

Answer

To assure 32-bit data, "Network Range Assignment" of the control station must satisfy the following conditions.
(1) The start device No. of LB is a multiple of 20H.
(2) The points assigned per station in LB is a multiple of 20H.
(3) The start device No. of LW is a multiple of 2.
(4) The points assigned per station in LW is a multiple of 2.
Product Name
Network Related Products
Series
CC-Link IE Controller Network

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries