FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Refresh timing of bit data and word data in the same CC-Link station
FAQ
Refresh timing of bit data and word data in the same CC-Link station
Sometimes the refresh timing of bit data and word data do not match in the same CC-Link station What is the cause?
- Category :
Answer
Cyclic data is sometimes separated into new and old data by two words (32 bits) with auto refresh timing. Checking "Block data assurance per station" of the CC-Link parameter setting "Operation Setting" assures the integrity of the cyclic data RX, RY, RWr, and RWw.
- Product Name
- Network Related Products
- Series
- CC-Link
May I have your opinion?
Related FAQ
- Mixing line topologies with star topologies in the CC-Link IE Field Network
- Data length for fixed buffer data communications by QJ71E71
- Using Ethernet UTP cables for the CC-Link IE Controller
- Limitation on the number of MELSOFT products that can be connected with the QJ71E71
- Link data from communication error stations in a CC-Link network