Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23082
  • Release Date : 2018/09/03 17:31
  • Update : 2018/09/26 13:15
  • Print

Assignment for connecting two CC-Link remote input modules (16-point type) (Remote net Ver.1 mode)

When I have connected two CC-Link remote input modules (16-point type) and set the remote input refresh device to "X100" in the remote net Ver.1 mode, what will the assignment of X devices be for each station?
Category : 

Answer

X devices will be assigned as follows. (With this setting, 32 points are occupied per station.)

 - Station No. 1: X100 to X11F
 - Station No. 2: X120 to X13F

The first 16 points of each station are used by a program.
Product Name
Network Related Products
Series
CC-Link

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries