FAQ
FAQAbout Products
- FAQ > Robots > Industrial/Collaborative Robots-MELFA > Ceiling mounted, holizontal type robot > The servo-on cannot be performed.
FAQ
The servo-on cannot be performed.
The servo-on cannot be performed.
Answer
Cause:
- A servo OFF signal(SRVOFF)is being input from an external source.
- The operating right is not given.(IOENA parameters settings/exclusive input and output).
- An error is occurring.
- TB operation error(enabling switch, activate/deactivate)
Measures:
- Check for a servo OFF signal and check the operation rights.
- Check how to operate the TB. Check that the 3 position enabling switch is set to the middle position.
- If an error message is occurring please cancel it.
- Product Name
- Industrial Robots MELFA
- Series
- FR Series
F Series