FAQ
FAQAbout Products
- FAQ > Robots > Industrial/Collaborative Robots-MELFA > Ceiling mounted, holizontal type robot > The position becomes offset.
FAQ
The position becomes offset.
•The position becomes offset during automatic drive.
•The position becomes offset after moving the equipment.
•The position becomes offset after moving the equipment.
Answer
Cause:
- Program error (arithmetic processing, etc.).
- Teaching operation error.
- Peripheral equipment is offset.
- There is a setting error in the origin position data.
- The origin position data has been lost(battery life, etc.).
- Origin positions are offset(the arm was moved while the power supply was OFF, etc.)
- Connecting parts have come loose.
- Belt teeth have been skipped.
- Increased backlash from the reduction gear.
Measures:
- Check the positioning data in the area where the positioning has become offset.
- Check the peripheral equipment and the robot's connecting parts(hand, robot installation section, etc.)
- Check the remaining time on the robot battery's life.
- Check the position of the origin positions.
- Check the condition of the belt.
- Check whether there is any nearby interference, etc.
- Product Name
- Industrial Robots MELFA
- Series
- FR Series
F Series
May I have your opinion?
Related FAQ
- Operation panel does not display anything.
- The operation panel does not light up. Although the T/B has got the electricity, the operation of T/B cannot be done.
- The servo-on cannot be performed.
- Brake is not working properly.
- In automatic drive mode, the system does not start up or the robot stops during automatic drive.