FAQ
FAQAbout Products
- FAQ > Robots > Industrial/Collaborative Robots-MELFA > Ceiling mounted, holizontal type robot > The leakage current breaker trips.
FAQ
The leakage current breaker trips.
•The leakage current breaker trips when the controller's primary power switch is turned ON.
•The leakage current breaker trips when the servo is switched on.
•The leakage current breaker trips when the servo is switched on.
Answer
Cause:
- Incorrect breaker selection(current capacity/drive purpose, etc.).
- Leakage current due to electrically conductive foreign matters(oil/moisture) getting inside.
- Earthing due to cable wear.
Measures:
- Check the specification of the breaker.
- Check whether or not electrically conductive foreign matters have got inside the robot's body or inside the controller.
- Check whether or not the cable is damaged.
- Product Name
- Industrial Robots MELFA
- Series
- FR Series
F Series
May I have your opinion?
Related FAQ
- The T/B does not display anything.
- The hand does not move properly (Electric operated hand).
- The communication fault occurs by the equipment connected to the Ethernet cable inside the robot arm.
- The operation panel does not light up. Although the T/B has got the electricity, the operation of T/B cannot be done.
- Oil is leaking.