FAQ
FAQAbout Products
- FAQ > Robots > Industrial/Collaborative Robots-MELFA > Ceiling mounted, holizontal type robot > Brake is not working properly.
FAQ
Brake is not working properly.
Brake is not working properly.
Answer
Cause:
[Occurs only when operating manually]
•T/B operation error.
•The enabling device input is open.
[Occurs when operating manually and automatically]
•Faulty connection of the cables that run between devices.
•Brake failure.
•T/B operation error.
•The enabling device input is open.
[Occurs when operating manually and automatically]
•Faulty connection of the cables that run between devices.
•Brake failure.
Measures:
[Occurs only when operating manually]
•Check the T/B operation(operation buttons, 3 position enabling switch, etc.).
•Short circuit the CNUSR connector’s enabling device input.
[Occurs when operating manually and automatically]
•Check the mating of the cables that run between devices.
•Check the T/B operation(operation buttons, 3 position enabling switch, etc.).
•Short circuit the CNUSR connector’s enabling device input.
[Occurs when operating manually and automatically]
•Check the mating of the cables that run between devices.
- Product Name
- Industrial Robots MELFA
- Series
- F Series