Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23284
  • Release Date : 2018/09/12 15:11
  • Print

About Low-voltage Power Distribution Products

What is voltage range that can be applied to a control coil of SR-T*and SRD-T* type?
Category : 

Answer

At ambient temperature 40℃, the rated voltage (frequency) is applied tothe control coil, and after temperature rise and saturation, it can operatewithout any trouble at 85 to 110% of the coil rated voltage. Whenapplying the voltage continuously, please use at 95 ~ 100% of that.
Product Name
Motor Starters
Series
MS-T/N

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries