Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23442
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/26 16:58
  • Print

Ethernet connection with QnUDVCPU

I want to connect a GOT2000 series model and the QnUDVCPU by Ethernet by using the Ethernet port built in the CPU.
How can I set it?
Category : 

Answer

The following describes an example of settings to connect a GT27, GT25, or GT21 model (Ethernet connection model) and the QnUDVCPU by Ethernet by using the built-in Ethernet port.

1. Configure the following settings in GT Designer3 (GOT2000).
◆ For GT Designer3 (GOT2000) Version1.100E or later
 (1) Select [Common] → [Controller Setting] → [CH1] from the menu.
   Manufacturer: MITSUBISHI ELECTRIC
   Controller Type: MELSEC-Q/QS, Q17nD/M/NC/DR, CRnD-700
   I/F: Ethernet:Multi
   (For GT Designer3 (GOT2000) Version1.170C or earlier, Standard I/F(Ethernet): Multi)
    [Standard I/F(Ethernet): Multi]
   Driver: Ethernet(MITSUBISHI ELECTRIC), Gateway
   (For GT Designer3 (GOT2000) Version1.178L or earlier, Ethernet (MELSEC), Q17nNC, CRnD-700, Gateway)
   GOT Net No.: 1
   GOT Station: 18
 (2) Select [Common] → [Controller Setting] → [CH1] → [Ethernet Controller Setting] from the menu.
   Host: *
   Net No.: 1 (example)
   Station: 1 (example)
   Unit Type: QnUD(P)V/QnUDEH
   IP address: 192.168.3.39
   Port No.: 5006
   Communication: UDP
 (3) Select [Common] → [GOT Ethernet Setting] → [GOT IP Address Setting] → [Standard Port] from the menu.
  (For GT Designer3 (GOT2000) Version1.170C or earlier, select [Common] → [Controller Setting] → [CH1] → [GOT Standard Ethernet Setting].)
   GOT IP address: 192.168.3.18
   Subnet Mask: 255.255.255.0

2. Configure the following settings in GX Works2.
 (1) Select [Parameter] → [PLC parameter] → [Built-in Ethernet Port Setting] from the menu.
   IP address: 192.168.3.39
   Subnet Mask Pattern: 255.255.255.0
 (2) Select [Parameter] → [PLC parameter] → [Built-in Ethernet Port Setting] → [Open Setting] from the menu.
   Protocol: UDP
   Open System: MELSOFT Connection

For the details, refer to the following.

・ GOT2000 Series Connection Manual (Mitsubishi Electric Products) For GT Works3 Version1 (SH-081197ENG)
 "5.3 GOT Side Settings"
 "5.4 PLC Side Setting"
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (communication)
Series
GOT2000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries