Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23457
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/25 20:51
  • Print

Gesture functions available for the historical trend graph

What gestures are available for the historical trend graph?
Category : 

Answer

The following gestures are available for the historical trend graph.

◆ GT Designer3 (GOT2000) Version 1.100E or later
・ Tap: Displays the cursor on the tapped position.
・ Swipe along the time axis: Scrolls the historical trend graph by half the page in the swiped direction.
・ Pinch in along the time axis: Reduces the time axis by one size (equivalent to the key code switch FFF9).  
・ Pinch out along the time axis: Enlarges the time axis by one size (equivalent to the key code switch FFF8).  

* Enlargement and reduction in size in the device value direction (along the vertical axis) with gesture operations are not available.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture), GOT function (historical trend graph)
Series
GOT2000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries