FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > System dialog display in the screen gesture mode
FAQ
System dialog display in the screen gesture mode
What operation is performed when the system dialog is displayed in the screen gesture mode?
Answer
When the system dialog is displayed in the screen gesture mode, enlargement or scrolling is canceled and the screen display returns to the normal size (100%).
Also, the screen gesture mode is canceled.
Also, the screen gesture mode is canceled.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture), GOT function (standard function)
- Series
- GOT2000 Series