FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT21 > PLC access from GX Works2 via the GOT
FAQ
PLC access from GX Works2 via the GOT
When connecting a personal computer (GX Works2) and the built-in Ethernet interface of Q03UDECPU via the USB interface of the GOT2000 series, how should I set the connection destination in GX Works2?
- Category :
-
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT21
Answer
When connecting a personal computer (GX Works2) and the built-in Ethernet interface of Q03UDECPU via the USB interface of the GOT2000 series, set the connection destination in GX Works2 as follows.
1. PC side I/F Serial Setting
・ Select [USB].
2. PLC side I/F Detailed Setting of GOT
・ CPU mode: Select [QCPU (Q mode)].
・ Select [via GOT(Ethernet) transparent mode].
・ Model: Select [Ethernet Built-in CPU].
・ IP address: Enter the IP address of Q03UDE.
3. Other Station Setting
・ Select [No Specification].
Note that the connection is not established unless the following conditions are satisfied.
・ Ethernet communication between the GOT and Q03UDE is properly established.
・ The connection destination of the transparent function is set to Q03UDE (MELSEC-Q/QS, Q17nD/M/NC/DR, CRnD-700).
For the details, refer to the following.
・ GOT2000 Series Connection Manual (Mitsubishi Electric Products) For GT Works3 Version1 (SH-081197)
"Chapter 5 ETHERNET CONNECTION"
"Chapter 23 FA TRANSPARENT FUNCTION"
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
"5.3.6 Setting target channels for the FA transparent function"
1. PC side I/F Serial Setting
・ Select [USB].
2. PLC side I/F Detailed Setting of GOT
・ CPU mode: Select [QCPU (Q mode)].
・ Select [via GOT(Ethernet) transparent mode].
・ Model: Select [Ethernet Built-in CPU].
・ IP address: Enter the IP address of Q03UDE.
3. Other Station Setting
・ Select [No Specification].
Note that the connection is not established unless the following conditions are satisfied.
・ Ethernet communication between the GOT and Q03UDE is properly established.
・ The connection destination of the transparent function is set to Q03UDE (MELSEC-Q/QS, Q17nD/M/NC/DR, CRnD-700).
For the details, refer to the following.
・ GOT2000 Series Connection Manual (Mitsubishi Electric Products) For GT Works3 Version1 (SH-081197)
"Chapter 5 ETHERNET CONNECTION"
"Chapter 23 FA TRANSPARENT FUNCTION"
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
"5.3.6 Setting target channels for the FA transparent function"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (FA transparent function)
- Series
- GOT2000 Series