Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23497
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/26 15:33
  • Print

Transferring data between a personal computer and a GOT via a PLC

Can the GOT screen data be read and written from and to a personal computer via a PLC?
Category : 

Answer

The GOT screen data can be read and written from and to a personal computer via a PLC.

Note that the following items have restrictions.
 ・ Connection type between the personal computer and PLC
 ・ Connection type between the GOT and PLC
 ・ Type of the PLC to be routed
 ・ GT Designer3 (GOT2000) version

The following items have restrictions depending on the type of the PLC to be routed.
 ・ Serial number of the PLC
 ・ Version of the engineering software (GX Works2)

For the details, refer to the following manual.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
   "4.4 Transferring the Data between the Personal Computer and the GOT via PLC CPU"

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (screen data transfer)
Series
GOT2000 Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?