Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23499
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/25 17:29
  • Print

Device data transfer between devices connected to the GOT

When Mitsubishi Electric and non-Mitsubishi Electric PLCs are connected to a GOT2000 series model, how can the device data of each PLC be transferred easily?
Category : 

Answer

The GOT2000 series allows device data to be transferred among multiple controllers (among PLCs, PLCs and temperature controllers, etc.).

For the details of the device data transfer function, refer to the following manual.

・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220)
 "9.4 Transferring Data between Devices ([Device Data Transfer])"
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (multi-channel function), GOT function (device data transfer)
Series
GOT2000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries