Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23518
  • Release Date : 2018/09/14 15:07
  • Update : 2018/09/26 15:22
  • Print

Vertical installation of the rugged model

Answer

The rugged model can be used vertically.
An arrow instructing the vertical installation is shown on the back of the GOT. Install the GOT vertically in the direction of the arrow.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Rugged model
Series
GOT2000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries