Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23535
  • Release Date : 2018/09/14 15:07
  • Update : 2018/09/25 17:15
  • Print

Optional UV protective sheet for the rugged model

When the optional UV protective sheet for the rugged model is attached, how much is the UV cutoff?
Category : 

Answer

When the optional UV protective sheet for the rugged model is attached, 99.75% of UV is cut off.
・ When the protective cover for oil is used: 0.05 × 1 = 0.05 (95% cutoff)
・ When the UV protective sheet is used: 0.05 × 0.05 = 0.0025 (99.75% cutoff)
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Rugged model, option (UV protective sheet)
Series
GOT2000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries