Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • No : 23537
  • Release Date : 2018/09/14 15:07
  • Update : 2018/10/04 13:29
  • Print

IP67F

Answer

The first digit of IP67F indicates the level of protection against dust (ingress of solid objects).
IP6□ indicates the dustproof type (a wire of 1.0 mm in diameter does not enter).
IP□7 indicates that the GOT is not subject to harmful effects by a temporary water immersion.
"F", the character at the end of "IP67F", is a symbol indicating oil resistance.
It is described in the appendix of the Japanese Industrial Standards (JIS) C 0920.
For the details, refer to JIS C 0920.
Product Name
Human-Machine Interfaces(HMIs)-GOT
Series
GOT2000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries