FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT21 > IP67F
FAQ
IP67F
What is IP67F?
- Category :
-
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT21
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT1000 Series > GT15
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT1000 Series > GT16
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT1000 Series > GT11
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT1000 Series > GT10
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT1000 Series > GT14
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25 Rugged
Answer
The first digit of IP67F indicates the level of protection against dust (ingress of solid objects).
IP6□ indicates the dustproof type (a wire of 1.0 mm in diameter does not enter).
IP□7 indicates that the GOT is not subject to harmful effects by a temporary water immersion.
"F", the character at the end of "IP67F", is a symbol indicating oil resistance.
It is described in the appendix of the Japanese Industrial Standards (JIS) C 0920.
For the details, refer to JIS C 0920.
IP6□ indicates the dustproof type (a wire of 1.0 mm in diameter does not enter).
IP□7 indicates that the GOT is not subject to harmful effects by a temporary water immersion.
"F", the character at the end of "IP67F", is a symbol indicating oil resistance.
It is described in the appendix of the Japanese Industrial Standards (JIS) C 0920.
For the details, refer to JIS C 0920.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Series
- GOT2000 Series