FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > GT25 Rugged > Location of the terminating resistor setting switch for the RS-422/485 communication port
FAQ
Location of the terminating resistor setting switch for the RS-422/485 communication port
Where is the terminating resistor setting switch for the RS-422/485 communication port located on the rugged model?
Answer
The terminating resistor setting switch for the RS-422/485 communication port is located inside the battery cover on the back of the rugged model.
For the details, refer to the following.
GOT2000 Series User's Manual (Hardware) (SH(NA)-081194ENG-X)
"4.3 GT2507T-W"
For the details, refer to the following.
GOT2000 Series User's Manual (Hardware) (SH(NA)-081194ENG-X)
"4.3 GT2507T-W"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model
- Series
- GOT2000 Series
May I have your opinion?
Related FAQ
- Checking the simultaneous 2-point press switches placed on the screen design software
- Operating the screen with the gesture function while using the SoftGOT-GOT link function
- Operating the objects with the gesture function using the SoftGOT-GOT link function
- Color of the rugged model metal body
- Using the rugged model in rain