Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23583
  • Release Date : 2018/09/14 15:09
  • Print

Torque limit

Answer

Set the torque limit value in "[Cd.101] Torque output setting value" before the positioning start.
The values of "[Pr.17] Torque limit setting value" and "[Cd.101] Torque output setting value" are compared, and the lower set value is valid.
Product Name
Simple Motion module/
Positioning module
Series
MELSEC-Q
MELSEC-L
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?