Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23606
  • Release Date : 2018/09/14 15:09
  • Print

Speed change during JOG operation

Answer

Yes. The speed can be changed during JOG operation.
Set the new speed with "[Cd.14] New speed value", and then set "[Cd.15] Speed change request" to "1".
Product Name
Simple Motion module/
Positioning module
Series
MELSEC iQ-R
MELSEC iQ-F
MELSEC-Q
MELSEC-L
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?