FAQ
FAQAbout Products
- FAQ > Controllers > Motion Controllers > MELSEC iQ-R Series > Simple Motion Modules > RD77GF > HPR request flag
FAQ
HPR request flag
When does the "HPR request flag" turn ON?
- Category :
Answer
It depends on the setting of servo parameter "[PA03] Absolute position detection system" whether the HPR request flag ("[Md.31] Status": b3) turns ON or not.
The flag turns ON in the following cases:
(1) "1: Enabled (absolute position detection system)"
• When the machine HPR has not been executed at the absolute position system
• When a machine HPR operation starts
• When the absolute system has not been set
• When "[PA14] Rotation direction selection/travel direction selection" is changed
• When changes of servo amplifiers or motor encoders are detected [RD77GF only]
• When the MR-J4-GF was not connected at the previous establishment of the home position for virtual servo amplifier connection [RD77GF only]
• When the electronic gear is changed [RD77GF only]
(2) "0: Disabled (incremental system)"
• System's power supply on or reset
• Servo amplifier power supply on
• Machine HPR start
• When the electronic gear is changed after HPR execution [RD77GF only]
The flag turns ON in the following cases:
(1) "1: Enabled (absolute position detection system)"
• When the machine HPR has not been executed at the absolute position system
• When a machine HPR operation starts
• When the absolute system has not been set
• When "[PA14] Rotation direction selection/travel direction selection" is changed
• When changes of servo amplifiers or motor encoders are detected [RD77GF only]
• When the MR-J4-GF was not connected at the previous establishment of the home position for virtual servo amplifier connection [RD77GF only]
• When the electronic gear is changed [RD77GF only]
(2) "0: Disabled (incremental system)"
• System's power supply on or reset
• Servo amplifier power supply on
• Machine HPR start
• When the electronic gear is changed after HPR execution [RD77GF only]
- Product Name
- Simple Motion module/
Positioning module
- Series
- MELSEC-Q
MELSEC-L