Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23627
  • Release Date : 2018/09/14 15:10
  • Print

Total capacity of servo amplifier to be connected to power regeneration common converter

When the total capacity of servo amplifier to be connected to FR-CV power regeneration common converter is like that of system which all axes do not operate at the same time, can I select the total capacity of the servo amplifier which all axes do?
Category : 

Answer

Select the total capacity of the servo amplifier to be connected.
For selecting combination of FR-CV power regeneration common converter and servo amplifier capacities, you need to consider the inrush current, etc. at power-on as well as during the operation. Refer to the servo amplifier instruction manual for selecting the total capacity and select the total capacity of the servo amplifier to be connected as specified.
Product Name
AC Servos-MELSERVO
Series
MELSERVO-J4, MELSERVO-J3, MELSERVO Others

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries