Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23706
  • Release Date : 2018/09/19 17:16
  • Print

The operating time of the instantaneous factor operating characteristics

Does the operating time of the instantaneous factor become 50 ms or shorter in both cases for 200% and 400% of the settling value?
Category : 

Answer

That is right. Standard JIS C 4602 defines it shall be 50ms or shorter when 200% of the settling value is input.
Product Name
Protection Relay
Series
MELPRO-A Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries