Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • No : 23708
  • Release Date : 2018/09/19 17:16
  • Print

A lighting condition of RUN

Answer

Because this relay derives the control power from input of the CT secondary current, when the input current falls below about 0.5 A for 2-phase input or about 0.7A for single-phase input, it will light out. When the current is around this range, because of fluctuation of current values, LED (RUN) will lights up/out repeatedly. That is not a failure.
Product Name
Protection Relay
Series
MELPRO-A Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries