Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 24684
  • Release Date : 2019/02/22 11:38
  • Update : 2019/02/22 15:03
  • Print

How to use built-in high-speed counters

I would like to know how to use built-in high-speed counters.
Category : 

Answer

For contacts to drive the coils of high-speed counters, use the contacts which are normally on during high-speed counting.
Do not use the input (X000 to X007) of the high-speed counters as contacts to drive the output coils (OUT) of the high-speed counters.
Product Name
FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
Product Category
High-speed Counting
Series
MELSEC-F series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries